7. Publish on behalf

Ingenuity offers the functionality to switch to another use so that you can manage the profile information or create posts on behalf of a colleague. To use this information, please contact the Ingenuity moderators to set it up for you. Once the setup is done, this works as follows:

Switch to another user

  1. Click on the burger menu
  2. Click on Switch to delegated profiles
  3. Click on the user name

Now you successfully switched to the delegated user profile. To double check, you should see the user icon of that delegated user in the header. You can use Ingenuity as always: manage the profile, create content or like and comment.

Switch user back

  1. Click on the burger menu
  2. Click on Switch user profile

Alternatively, you can click on the user icon in the header.